Inserting New Scripts
To insert a new script application and script, follow these steps.
|
1.
|
Open the document where you want to insert the script. It can be a new or existing document. |
A script application is inserted, and the Script Title dialog box opens.
Note: The TI-Nspire™ CX Student Software and the TI-Nspire™ CX CAS Student Software open automatically within the Documents Workspace.
|
3.
|
Type a script title. (The maximum number of characters is 32.) |
The Script Editor window opens showing a blank script.
|
5.
|
Type your text in the script lines. |
Note: Some nonstandard UTF-8 wide characters may not be displayed correctly. For these characters, it is highly recommended that you use the string.uchar function.
|
6.
|
When the script is complete, click to execute it. |
|
•
|
In a TI-Nspire™ document, the script application is inserted in a new page. When the page containing the script application is active, the Documents Toolbox is empty. |
|
•
|
In a PublishView™ document, a frame containing the script application is added to the active page. You can move or size this frame just as you would any other PublishView™ object, and you can add other PublishView™ objects to the page. |
|
7.
|
To view the script application, click. |
Zooming Text in the Script Editor
You can adjust the size of the text in your script and in any of the tool panels.
Menu Method
|
1.
|
Click in the area of the text to zoom. |
|
2.
|
On the menu, select , and then select , , or . |
Note that the menu also displays keyboard shortcuts for the Zoom commands.
Mouse Method
|
3.
|
Postion the mouse pointer over the area to zoom. |
|
4.
|
Hold , and roll the mouse wheel forward or back. |